STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hard fault caused by unaligned access

Hi, I have an issue when trying to copy a struct by direct assignment on STM32H743; The code:   void function(const structName_t *incomingStruct) { Signal_t sendSignal; sendSignal.desiredStruct = *incomingStruct; // <-- Causes unaligned access .....

RBrec.1 by Associate III
  • 19473 Views
  • 23 replies
  • 4 kudos

STM32U5 LL example ADC1 and ADC4

The example project does not provide information on ADC4 register configurations, ADC4 seems to be different then prior peripherals (e.g. compared to L4).  ...\NUCLEO-U575ZI-Q\Examples_LL\ADC\ADC_SingleConversion_TriggerSW_IT_InitSTM32CubeMX configur...

edw by Associate
  • 2626 Views
  • 0 replies
  • 1 kudos

spi slave weird data on mid-high speeds ?!

I am having weird issue with STM32F767 (configured to run at 200mhz) that needs to be SPI slave .. I configured it with 0,1 (clock low, second edge), hardware cs.. when master sends data at 350kbps everything is ok, when master sends at higher speeds...

arhi by Associate III
  • 9807 Views
  • 24 replies
  • 1 kudos

Can VDDA VREF+ and VssA connect to VSS(ground)?

I am using STM32H735,TFBGA-100 controller with 550MHz.I don't need ADC and DAC functions.1.Shall i connect VDDA,VREF+ and VssA to ground(Vss)? if yes, what is the recommended(through any resistor or  shorted)way to connect to Vss?2.If i did as above,...

Resolved! Weird Jitter when using DMA to generate PWM in GPIOs

So i was trying to generate pwm on all gpio pins of a stm32F103 for my application. I found followed this guide:https://www.hackster.io/javier-munoz-saez/all-pins-as-pwm-at-the-same-time-baremetal-stm32-1df86f the essence is using the function:      ...

Okbit_0-1702369391874.png Okbit_1-1702369391855.png Okbit_2-1702369391867.png
Okbit by Associate II
  • 2910 Views
  • 4 replies
  • 3 kudos

STM32L552 Azure RTOS ThreadX UART RX+TX not working correctly

Hi together,at work I have an Azure RTOS based project with UART communication. The basic implementation of ThreadX is working fine for toggling LEDs, but I need to do some SPI communication to an ePaper display and communicate with the MCU over UART...

BViet1_0-1701950414458.png
BViet.1 by Associate III
  • 4414 Views
  • 2 replies
  • 0 kudos

Resolved! Configure ADC sampling frequency STM32H723ZG

Hi All,I am using a STM32H723ZG Nucleo board. I am using the ADC in 8-bit mode. The clock is set to 96 MHz, and according to the application note it should use 6 cycles to sample and convert which would result in 16 Msps, but it seems to be between 8...

elso_0-1702459071410.png
elso by Senior
  • 1803 Views
  • 1 replies
  • 1 kudos

Resolved! can bus ack signal

I want to scan (acquire) data from a vehicle can bus.1. Is it possible to prevent the ACK bit from occurring in CAN communication in the MCU?2. If I set the ID to receive all data, won't an ack occur?

YPark.5 by Associate II
  • 4060 Views
  • 3 replies
  • 1 kudos