I have a software update project and I have two different codes. I want to combine the hex files of these two codes into a single file and finally lock the processor with the help of Option bytes. How can I do this?
With the Stm32l443 processor family, data is received in 2-second periods over the LPUART interface. LPUART stops falling indefinitely during interruption. Uart deinit - it fixes itself when I do init.
Google does not find the site safe. I removed all firewalls but it still refuses to download. There was another way to download it. Any chance of sharing via email or github?