STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Accurate understanding of "STM32G491CCU6" ADC DMA1, ADC DMA2

Now I'm using the "STM32G491CCU6" MCU.It uses 5 and 4 channels of ADC1 and ADC2, respectively, while also using DMA.However, I configured it to use Rank and make DMA interrupt, and when writing code through STM32CubeIDE, I set "HAL_ADC_Start_DMA" and...

Park by Associate II
  • 1124 Views
  • 0 replies
  • 0 kudos

Syncing external ADC / DAC Conversions

Just wondering if anyone has information on how to sync external ADC and DAC conversions?The ADC and DAC are connected as SPI peripherals (separate SPI's) to an STM32G474RE.The system needs to run in continuous mode with a configurable delay between ...

Resolved! STM32G474 I2C Write/Read to the Flash Memory

Hi folks,I would like to use the I2C serial communication protocol to write/read from the Flash Memory using the STM32G474 microcontroller. I am using the B-G474E-DPOW1 board which does not have an EEPROM. Is it possible to achieve this goal or do I ...

gshet1 by Associate II
  • 3929 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F103RB UART comm. in half-duplex, single-wire mode

I am using two NUCLEO-F103RB boards for implementing and testing single-wire, half-duplex UART communication in polling mode. First I implemented and tested code based on the ‘UART_TwoBoards_ComPolling' example, which is included in the STM32F1 HAL l...

_legacyfs_online_stmicro_images_0693W00000dJxwmQAC.png
Kmax18 by Senior II
  • 9241 Views
  • 3 replies
  • 2 kudos

Resolved! How to temporarily disable timer outputs on STM32G071

In my application I have TIM1 configured to output a configurable frequency - which works well.Now I want to add support for pausing the timer and the outputs should then go to inactive state( = low).But whatever I try with MOE, OSSI, CC2E, CC2NE bit...

b.a. by Associate III
  • 7695 Views
  • 6 replies
  • 0 kudos