STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Happy 2024 !

To our valued community around the world, our warmest wishes for a happy, healthy, and prosperous new year! Top 3 Contributors and superusers during 2023 for the last 6 months and the new community @TDK with 326 solutions@Tesla DeLorean 151 solution...

2024_Happy.png
STOne-32 by ST Employee
  • 5668 Views
  • 5 replies
  • 18 kudos

Resolved! STM32U575 FW update over USB Type-C

Hello.For my project I'd like an option to update firmware on my STM32U575 over USB Type-C connector either with the computer or with the USB flash drive.Details:Board I'm developing has its own power, no power needed from USB. When connected to the ...

ATroš.1 by Associate II
  • 2907 Views
  • 3 replies
  • 0 kudos

Resolved! Can RCC_LSCO be pulled to ground without issue?

Hello,We have the RCC_LSCO of the U5 connected to a peripheral that warns that it will pull this line to ground when the peripheral itself is reset. At the moment, the pull strength of this peripheral is unknown, but let's say it's fairly strong.Does...

EC.3 by Associate III
  • 1845 Views
  • 5 replies
  • 0 kudos

Resolved! Flash sector erase is taking too long

Hi all i'm developing a bootloader on a stm32f407. I want to erase all the flash sectors except of the first 3 which i have the bootloader code. The problem is that to erase a sector it takes 1 second and i have an external watchdog on the board tha...

td by Associate II
  • 6478 Views
  • 9 replies
  • 2 kudos

Sending messages using SPI peripherals - stm32f746zg

Hi, I'm using stm32f746zg board, and I need to send message from spi1(full duplex master ) peripheral to spi2( full duplex slave) peripheral (on the same board) and then back to spi1. Also i want to use interrupts/DMA.1) If the message length is unkn...

Jordalic by Associate II
  • 1713 Views
  • 1 replies
  • 1 kudos

Resolved! CAN learning

I'm interested in learning about CAN. Please suggest me any course or other tutorials to start learning

jsw2000 by Associate II
  • 2405 Views
  • 3 replies
  • 0 kudos

Resolved! What's the difference between AHB, AHB1 and AHB2?

I read in reference manual and web tutorials of stm32f103c8, there were "AHB", "AHB1" and "AHB2", what's the difference between them, I know "APB1" and "APB2" are 2 APBs, the "1" and "2" are sequential numbers, how about "AHB1" and "AHB2" are they al...

MQi.1 by Senior II
  • 7869 Views
  • 2 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.