2023-06-18 3:32 PM
I've installed the usb drivers downloaded here but I still can't detect my STM32F103c6 board on the Device Manager on Windows 11. When trying to debug my first program on IAR I also got the error "Fatal error: Failed the search for probes, ensure that the USB drivers are installed. Session aborted!" and as I was searching on the internet it has to do with the lack of drivers. I also installed STM32CubeProgrammer as suggested in this forum and tried to update firmware but no device is shown on the "STLinkUpgrade" screen. So my question is do I need to install anything else? What am I missing? How do I make windows 11 detect my board? Thanks in advance.
2023-06-19 1:56 AM
So, is there a ST-LINK?
2023-06-25 6:01 AM
Yes (now there is, I wrongly assumed that the chip already comes shipped with a debugger since it has a USB cable but it doesnt). I bought a ST-LINK V2 and connected correctly the 3V,ground,SWCLK and SWDIO respectively. Now it appears on the device manager. However I'm still not able to do some live debugging. On the STM32Programmer I've got this error:
and in IAR when I click Download and Debug this error:
Sun Jun 25, 2023 09:56:06: : Fatal error: ST-Link, No MCU device found Session aborted!
2023-06-25 9:01 AM
Photo of the st link v2 mini
2023-06-25 9:09 AM
2023-06-25 11:28 AM
This is an illegal clone of the ST-LINK/V2, its behaviour is unpredictable, which has also been discussed very often here in the community. I recommend you get an original ST-LINK/V2 and try again with it.
2024-05-06 1:29 AM
Let me start by saying that I am a professional, not a young hobbyist tinkering around.
In my armory I have the "useless" STLink V3", 3 or 4 STLink V2s and isolated STLink V2.
During the pandemic I couldn't find STLink for my students from any distributor and I must admit that I ordered 10 Chinese ones complete with identical cases.
It is ridiculous, however, that still, after years and after investments that now almost monopolize the market, ST does not opensource its programmer. It is used with its microcontrollers and there are those who have now imitated it, reproduced it and on occasions it works even better than the original, and I'm not joking, BETTER THAN THE ORIGINAL! I have a very bad experience with new hardware that couldn't be programmed for unknown reasons with an original V2, while the Chinese one was working like a charm.
You would be better off focusing on serious things, such as the bugs that arise in the libraries that you give to improve and "speed up" the work and then bring entire projects into crisis.
I don't think you need the few pennies a programmer earns you...
2024-05-06 2:43 AM
@Msolinas The topic of why STMicroelectronics does not support the illegal clones has already been addressed here and does not belong in this thread. It is also not about making money with the original ST-LINK, but solely about the expectations of users who then wonder why their ST-LINK does not work (precisely because it is a clone) with software created by STMicroelectronics.
Nevertheless, thank you for your suggestions.
Regards
/Peter
2024-05-06 3:23 AM - edited 2024-05-06 3:33 AM
Opensourcing ST-Link won't yield any profit to ST. More important, this would disturb their valuable ecosystem partners. ST's investment in OpenOCD is very appreciated.