STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TOUCH GFX STRECHED CIRCLES

We have a dial gauge in the center of the screen and are getting stretched-out images of the dial, What is the solution to keep it in 1:1 ratio?MCU-STM32F750TFT-50 PIN 800X480BIT DEPTH-16BITIDE-STM32CUBEIDE 

ZExpo.1 by Senior
  • 2389 Views
  • 3 replies
  • 2 kudos

Resolved! How can I use multiple USB device classes with STM32L4

Hello together,does anyone know how I can implement multiple USB device classes on a STM32?I want to use the CDC so a VCP and the DFU class so I can communicate with my chip and drive an update if needed. I am working with a STM32L452RE.It must be po...

EniRot99 by Associate III
  • 4824 Views
  • 5 replies
  • 5 kudos

Resolved! STM32U5xx: thank you for a really "cool" MCU

Dear STM32 team,I want to thank you, honestly, for a really great MCU chip. Well done.(just as my friendly feedback to you and company)When I say, the STM32U5xx is a really "cool" MCU - I mean two things:It is really cool, in terms of temperature:I a...

tjaekel by Lead
  • 4108 Views
  • 6 replies
  • 6 kudos

L4 CRC and U5 CRC diff

Hi, I have both stm32u5 and stm32l469. I found that there are some differences in the CRC caculation.On stm32l469:if i configure the parameter as following, function hardware_crc32_calculate_with_seed works fine, no matter the code in line 185,186,19...

shwzh1990_0-1705868542338.png shwzh1990_2-1705868760679.png shwzh1990_3-1705868912631.png

DMA performance gain on SDIO

I am using STM32CUBE ide and my project has SD card access via SDIO peripheral.I am using FatFS middleware. To use FreeRTOS I enabled DMA and system works fine.After enabling the DMA I wanted to see how much read/write performance the system gained.I...

ASay.1 by Associate II
  • 1879 Views
  • 2 replies
  • 1 kudos

PLL is enabled on power on?

I'm trying to migrate my code away from Platformio, which I've previously been using, to cmake (currently using it with clion and openocd).I've got everything working but when I run my code I run in to one problem.For some reason the PLL is enabled a...

Dvan8_0-1705517684970.png
Dvan .8 by Associate II
  • 2372 Views
  • 3 replies
  • 1 kudos