STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Internal ADC questions on stm32h750

Hello,I am using an stm32h750. I have an ADC group that includes 4 inputs from GPIO ports and the 3 internal ADCs (VBAT, CPU Temp, Reference Voltage). It's set up with DMA. The conversions run at 150hz.We use a coincell battery voltage as input to VB...

F767 CAN Bus issue

Hi,I have an issue with the CAN1 controller in my MCU. I have connected the CAN transceiver to PA12(TX) and PA11(RX). When connected to the CAN Bus I can see the frames coming to the MCU(RX line) and the ACK bits are visible on the TX line. Unfortuna...

SD Card SDIO not working(FR_DISK_ERR)

I have a custom board and I have to run an SD card on it using SDIO protocol however on f_mount() function it takes a long time to come out with error FR_DISK_ERR but when I call "HAL_SD_GetCardInfo(&hsd, &sdCardSpace)" then I am getting all the data...

fs by Associate
  • 1375 Views
  • 2 replies
  • 0 kudos

Resolved! Octal SPI Interface

Hello Team,We are considering STM32H562ZIT3QTR MCU for our design. There will be two Microcontroller in our design.MCU consists of one Octal SPI Interface. Can other Microcontroller be interface with STM32H562ZIT3QTR through Octal SPI or we can only ...

kadam by Associate II
  • 2194 Views
  • 3 replies
  • 1 kudos

SMT32F407VGT6 / CAN issue

主控板 (SMT32F407VGT6)与同服板 (STM32F407VGT6) 之间的CAN通讯,环境温度低于-10度,通讯不正常,环境温度高过-10度!

JACK00 by Associate II
  • 2285 Views
  • 4 replies
  • 0 kudos

Resolved! I can not send message from PCAN to STM32F407VGT-DISC1 board.

Dear all,I set up a configuration to send message from ST board to PCAN USB and the other way around. When I send message from board to PCAN, it works just fine. I can see in the PCAN-View screen that the message is received successfully as shown bel...

demir_0-1706501897116.png demir_1-1706502067615.png demir_0-1706502382005.png
demir by Senior II
  • 3465 Views
  • 5 replies
  • 2 kudos

How to trigger a timer / DMA / ADC acquence with a comparator

I am currently using a nucleo g474re board to acquire 10,000 samples from an ADC using a timer and DMA.The timer allows me to use any data rate and the DMA puts the samples into memory without CPU intervention.The process is currently initiated by st...

LHarm.1 by Associate III
  • 1981 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F103: Intended behaviour of HAL_ADC_Start_DMA

I have a program where I am trying to scan over 8 ADC channels on ADC1, take 10 samples from each and transfer to the DMA. From everything I have read, I cannot enable DMA Continuous Conversion on STM32F103, so I will need to use discontinuous scan m...

WTetl.2 by Associate II
  • 9920 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.