Skip to main content
pvall.1
Associate III
October 4, 2023
Question

System bootloader

  • October 4, 2023
  • 1 reply
  • 721 views

Hello,

I'm currently working on a system bootloader using an STM32L4P5VGTx board. During this process, the board entered an unknown state and doesn't seem to recover even after a reset.

I also attempted to use the Cube Programmer tool to load a bin file, but it's not detecting the USB port for the connection and uploading process.

Could you please provide guidance on how to resolve this issue and bring the board back to normal operation?

This topic has been closed for replies.

1 reply

TDK
October 4, 2023

Custom board? Is the board connected with SWD? If so, you should be able to connect under reset.

"If you feel a post has answered your question, please click ""Accept as Solution""."