cancel
Showing results for 
Search instead for 
Did you mean: 

Not expected frequency on NUCLEO-L496 RTC output calibration

Sirac
Associate III

Hi,

I'm trying to improve the accuracy of RTC. For that, I use the AN2604 witch describe this.

But, when I activate the calibration output of RTC at 512Hz, I have only 496Hz at the output. (AsynchPrediv =127). I tried this simple code to the nucleo-L476 and I have a perfect 512Hz clock.

On the L496, if I change AsynchPrediv to 124 and I can see a frequency around 512Hz.

What could be wrong with the L496?

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Sirac
Associate III

I change the board of L496 and again, same frequency. So I change the crystal, the frequency is slightly better (504Hz) but too far from 512Hz.

I hope there is no trouble with MCU itself

waclawek.jan
Super User

Try an external oscillator with LSE, e.g. a signal generator (setting LSEBYP, see External source (LSE bypass) subchapter in RM).

JW

Good Idea, I test that asap

Thank's

mbarg.1
Lead

I have similar issue with Nucleo-H723G boards - i have 4 of them - LSE is runnig around 30800 Hz

try:

1. set LSE drive to high

2. make the caps on crystal smaller...what C-load your crystal should have?

If you feel a post has answered your question, please click "Accept as Solution".

I have the problem on Nucleo-H723G boards with default (cubeIde 13.1) setup.

We use official demo boards with official demo sw to avoid discussions on hw/sw.

waclawek.jan
Super User

Please don't hijack threads.

Start your own thread stating the problem, what hw and what sw exactly (what is official demo sw?) did you use and how exactly do you detect the problem.

JW

mbarg.1
Lead

Sorry for mixing apples with potatoes...

I will open a new topic asap.