STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The oscillatoris not working STM32F103CBU6TR

Hi,I'm using STM32F103CBU6TR and I see that the oscillator that connects to osc_in and osc_out is not working.The NRST is ih high, the BOOT0 is low and the power to the device is good.What is the problem?BRShmuel

SIlia.1 by Associate II
  • 2731 Views
  • 5 replies
  • 1 kudos

Resolved! Make an oscilloscope using stm 32

Hi, everyone I am Talha an Electronics student, I was recently working on making an oscilloscope using STM 32. I recently made a logic analyzer using stm 32 f103 RB. I now wanted to make a simple oscilloscope that simply displays the function generat...

Resolved! H743VI - pin dies away -- reliability problem of chip ?

Hi,Just yesterday on my H743VIT6 (rev. V ) on the running TFT : picture faded away...white screen.I just happened to look at the display , thinking ...ok, maybe one of the thin wires just broke now...TFT (small, 1,8" , ST7735 on 3,3V) connected /sold...

AScha3_0-1707651489653.png
AScha.3 by Super User
  • 3565 Views
  • 4 replies
  • 2 kudos

Resolved! STM32H563ZITx series ADC conversion-Reg

Tried implementing ADC conversion on STM32H563ZI Nucleo board. But, getting only a constant value like 66,67,68,69 in serial monitor(Tera term) irrespective of the given input even the i/p is unplugged getting the same values. Need a help to fix this...