STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Interrupt problem on stm32f7 (bare-metal)

Hello, I would like to contact you because, following the code made on Keil uvision 5, I cannot get my interrupt to work.Objective of the code, turn on and off the LED (pb0) of the card with the button (pc13) on it itself.PCB Used : STM32F767ZI

Nucleo-F207ZG UART issue

Good day I am not sure what I am doing wrong as I was quite successful on other dev kits to import examples. I have downloaded en.stm32cubef2-v1-9-4 from the ST website and I am trying to import some of the examples from th eProjects->NUCLEO-F207ZG->...

SDu T by Associate III
  • 4942 Views
  • 8 replies
  • 0 kudos

STM32 timeline infographics

Is there a newer version of this infographics:https://community.st.com/t5/image/serverpage/image-id/44904i6E7E4466B43E7167/image-size/large?v=v2&px=999?It was used in the "10 years of STM32" campaign.If there is no such, can please such infographics ...

HID host USB for getting barcode from a scanner.

HiI use HID host as USB profile for getting barcode from scanner (ES4650 scanner).I use STM32F746.Most of the time I get the right barcode, but sometimes it misses a character .I tried giving its interrupt the top priority, but it didn't solve the pr...

Ofer by Senior
  • 3469 Views
  • 3 replies
  • 3 kudos

STM32U5A5 -- I2C Timeout waiting for TXIS flag --

Hello all,I have been trying to get I2C communication working on my NUCLEO-U5A5ZJ-Q board based on STM32U5A5ZJJT6U. First I have used STM32-CUBE-IDE and CUBE-MX to generate code but I was getting error when I try to transmit so I write a custom code ...

ahsank by Associate II
  • 9444 Views
  • 11 replies
  • 0 kudos

STM32 celebrates 10 years of innovation

Posted on July 03, 2017 at 17:16     STM32 celebrates 10 years of innovation   From STM32F1, the world first 32-bit ARM� Cortex�-M MCU announced on June 11th to STM32H7, the world most efficient MCU released in 2017, the STM32 ARM� Cortex�-M microco...

0690X00000603vYQAQ.jpg 0690X00000603vYQAQ.jpg 0690X00000607OTQAY.png 0690X00000607HEQAY.png

STM32F405 UART communication between PC

I am sending a command to the STM32F405 through the UART (COM) port for receiving data from the STM32F405. Once the command send from PC it will continously send data from STM32F405. What if the PC drops the connection and goes to sleep. And my STM32...

cjaya.2 by Associate II
  • 2288 Views
  • 3 replies
  • 1 kudos

Unable to send data over USART1 TX line (PC4) on NUCLEO-G0B1RE

Hi,     Configured PC4 and PC5 for transmitting and receiving over USART1.    Enabled the interrupt, DMA is disabled.     Tried with different baud rates, same results.     The data seen on serial console application cutecom does not match data I am ...

mohitmg by Associate II
  • 2723 Views
  • 5 replies
  • 1 kudos

Resolved! About libraries and SDKs

We are developing using the following development environment. Are there any libraries or SDKs that we can use?Also, Is HAL or LL a library? [IDE] STM32CubeIDE 1.14.0[MCU] STM32F412VGT6