STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RTC configuration of outpot ALRM

Hello st community,I work on stm32h7, and I use with RTC output alarmA, when the MCU power supple turned off, and RTC work with VBATT to wakeup some component with this signal, but this component needs any pules to wakeup and not woke up with first e...

dToub.1 by Associate
  • 5142 Views
  • 9 replies
  • 0 kudos

Resolved! fast consecutive ADC Sampling for large chunk of data

Hi Everyone, in my previous posts i pretty much beat the bush around this subject and i did get some good supportbut i keep getting stuck with this issue.im using STM32H743ZI2 Evaluation board set to 32Mhzthe ADC is 16 bits and running on "fast chann...

shahaf321_1-1707384861260.png shahaf321_0-1707384421185.png
shahaf321 by Associate III
  • 3956 Views
  • 4 replies
  • 3 kudos

Resolved! Contradiction in Reference Manual RM0394

There is an inconsistency in RTC shadow register update frequency description. Some places in text mentions that shadow register update happens once every RTCCLK period:34.3.5, 36.3.4: "Every RTCCLK periods, the current calendar value is copied into ...

Resolved! spi problem communication STM32F103c8t6

Hello, i have a problem with my spi communication i don't recieve the information from the slave to the master Master configuration :Slave configuration : I want to receive how many time my led blink and i want to write it on my lcd screen. But every...

master.png masterclock.png spislave.png spiclock.png

Bit SCUEN of PWR peripheral of STM32H7

We don't understand the bit SCUEN of STM32H7. The description is not very clear:   Could you explain what SCUEN means and if the software is supposed to write or read this bit and why ?

Gpeti_0-1707468529159.png Gpeti_1-1707468601674.png
Gpeti by Senior II
  • 2959 Views
  • 5 replies
  • 3 kudos

STM32F401 Firmware Update via Wiznet W5500

Hi,For a project I am using a Wiznet W5500 ethernet chip with STM32F401RET6 MCU to exchange data via HTTP over ethernet with a Windows/OSX software application. The W5500 handles the ethernet communication and speaks to the STM over SPI, which all wo...

EVE by Associate
  • 2261 Views
  • 1 replies
  • 0 kudos

Resolved! Flash endurance parameter

Hi,Can somebody please explain what the "Flash memory endurance" value in the datasheet means? The max number of overall writes to the flash page or the max number of writes in the particular "cell" inside the page?Simple context:Let's say that the M...

kvrbek by Associate II
  • 2910 Views
  • 2 replies
  • 1 kudos