STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Porting WICED sdk from STM32F423 to STM32U5A5

Good morning, I have to do a porting from a project developed on STM32F423 to an STM32U5A5The starting project used the wiced sdk, with the supported platform STM32F423.If I understand well, for STM32U5A the wiced sdk is deprecated, and it would be b...

CORDIC COS implementation

https://github.com/Sushmitabaga/CORDIC/tree/main  I  was trying to Enable CORDIC IN STM32G4 series  for  checking the time taken by normal cos function and cos CORDIC function.  But i found that both are taking almost the same time. which is not poss...

Sushmita by Associate II
  • 5854 Views
  • 9 replies
  • 2 kudos

Resolved! No activate option of timer in STM32CubeIDE CubeMX

Hello, I am working with "Mastering The STM32" book and faced with one problem: cannot find the option as in the book to activate any timer using CubeMX. I am using STM32 blue pill STM32F103C8T6. Why I can't find the activate option of timers?

Resolved! NUCLEO H743ZI2 MB1364E and MB1364C

Hello, I hope you are doing great.I have two NUCLEO H743ZI2, one of them is MB1364E, and the other one is MB1364C. They are totaly the same but there are little differences and I would like to find them and make them same, since I would like to use t...

Waking up from RTC on a STM32G030

Hi all,I'm struggling for days why my RTC wakeup doesn't work.The program is running FreeRTOS, but I want the uC in Lowpower Sleep for 3 minutes.So I set RTC on 1Hz, counter 180 and internal wakeup.Activated the EXTI RTC interrupt.But it immediately ...

WSpar.1 by Associate III
  • 2957 Views
  • 3 replies
  • 0 kudos

about Execute in place using dual quad spi

What I want to do is XIP with DUAL QUAD SPI.The environment is as follows.Use Board : nucleo l4r5ziIDE : Atollic TrueSTUDIO® for STM32, Built on Eclipse Neon.1a.(Version: 9.3.0)FLASH : W25Q64JVThe connection diagram of the board and FLASH is shown be...

Myasu1_0-1708448593094.png Myasu1_0-1708697574834.png Myasu1_1-1708698042431.png Myasu1_2-1708698571213.png
Myasu.1 by Senior
  • 6616 Views
  • 9 replies
  • 1 kudos

tft RGB close pins

hello i wand to use stm32h7 series LQFP package to connect RGB888 display first time i try with this chip   the alternate pins is not close to each other.. and for optimal high speed pcb traces, it be nice this pins to be close or im mistaken and not...

Lios by Associate II
  • 745 Views
  • 0 replies
  • 0 kudos