Hi ! Im new to STM and have to write a 180 Degree conduction code using CUBE IDE need help Im also attaching a code that I wrote for Tiva. Please help out Could use any pins available in STMSTM Board : STM32F407VGT6 MCU Discovery board #include "TM4...
Hi,I am a beginner and I want to generate a 50Hz square wave on STM32F407 on Keil UVision4Please mention libraries etc that are being used and if you can how to add them to Keil UVision so it doesn't give an error.
I will try this rn and get back to you Thank you smPlus do have any videos or resources that can help me in learning how to use stm32cube ide to accomplish the task or can you explain it
I have to use the Board STM32F407VGT6 and the example offers to measure an external signal while I want to output a square wave on any of the output pins of the board without any external signal. Could you please guide how to do that
Thank you sm for this ! I am a student and this helped me a lot I justneed a little help can you please guide me what the value of the system clock is and how I can change the output to 50Hz square wave or any value of hz for a square wave.