STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configure GPIOs PA11 and PA12 to USB D+ and D-

Posted on July 11, 2016 at 17:27I'm working with STM32F070xBI need to configure GPIOs PA11 and PA12 to USB D+ and D- alternate function. According to datasheet it is listed as Additional functions (not Alternate) USB_DM and USB_DP. It is not clear h...

dimax by Senior
  • 2649 Views
  • 4 replies
  • 0 kudos

Resolved! Brown Out Reset in STM32H753ZI

I am using STM32H753ZI for my project. My use case is I want to detect brown out reset after brownout occurs and system restarts.I am checking brownout reset flag using if (__HAL_RCC_GET_FLAG(RCC_FLAG_BORRST). My query is this flag is shared/common b...

A3 by Associate III
  • 1793 Views
  • 1 replies
  • 1 kudos

I2C does not work when FMC is turned on

Hi,I am using STM32H743II microcontroller. In which  communicating with external SRAM with FMC. It is working fine.I need to communicate with the touch LCD IC via I2C. There is no problem in communication when FMC is not active. I am reading the touc...

OKose.1 by Associate
  • 2346 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H7xx SPI. Tutorial, documentation or example code needed.

I need to write firmware for STM32H7xx to interact with an SPI flash memory chip. (STM32 master, 8-bit, full-duplex polling, no CRC and application controlled #CS.) I am using STM32CubeIDE 1.14.0 and used the device configuration tool to produce my S...

JBend.6 by Associate III
  • 19916 Views
  • 12 replies
  • 1 kudos

Custom bootloader on the STM32L4

​Here's how I implemented a custom bootloader using the STM32L475. I thought I would share since I have seen so many posts from people having issues invoking their application from their bootloader.​I attempted to post this as an idea in the knowledg...

Stanford by Associate II
  • 7207 Views
  • 2 replies
  • 2 kudos