User Activity

HiEarlier today I was demonstrating a IAP functionallity with dualbanking on a stm32G474RET. I was saying that it cannot fail as I check the written image with a CRC after it has been written to the new bank.As I power of the system mid transfer and ...
HiAssume that i set up an H-bridge and and control it via the HRTIM block and use the build in deadtime features. I then also enable a couple of faults. The bridges safe state will be to set both lower transistors to be OFF and the two upper once to ...
Kudos given to