STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ARMv4 instruction "ADC R0, R1, LSL #1" not recognized

I am using STM32CubeIDE 1.15.0, writing code in C, including some assembler code, for the STM32G431.According to ST's programming manual PM0214 in Section 3.5.1, I should be allowed to useadc r0, r1, lsl #1However, gcc barfs (I am using standard gnu1...

Hansel by Senior
  • 3848 Views
  • 5 replies
  • 3 kudos

DAC via opamp follower

Hi all,I am in the process of bringing up a prototype board with a STM32L4R7ZIT6 up. I'm using one DAC channel via the opamp. This is working all right, until I designate the default output of the DAC to another function e.g. dig output. The DAC is c...

GeertZelf by Associate III
  • 8105 Views
  • 10 replies
  • 0 kudos

IWDG resetting when making the window larger

- STM32G0B0RE     Our controller was running fairly well but on occasion we were seeing the windowed watchdog trip(The IWDDGRSTF flag set on reboot.) We were not sure whether this was a too short or too long trip so decided to extend the window wider...

Resolved! STM32L072 USB

Hi all,A USB device should pull up DP when it detects VBUS power only. This is described in the USB standards and ST AN4879 factsheet. Question 1. Is there any other (smarter) way with the STM32L072 than to monitor VBUS power on a GPIO yourself (via ...

JanAtze by Associate II
  • 3462 Views
  • 7 replies
  • 0 kudos

Resolved! what does the status codes mean, how do you read them ?

here are the functions:/*** @brief Return the OSPI error code.* @PAram hospi : OSPI handle* @retval OSPI Error Code*/uint32_t HAL_OSPI_GetError(const OSPI_HandleTypeDef *hospi){return hospi->ErrorCode;}/*** @brief Return the OSPI handle state.* @PAra...

MNapi by Senior III
  • 2100 Views
  • 2 replies
  • 2 kudos

Resolved! stm32h747 GETCHAR_PROTOTYPE strangeness

Hi Guys,This is driving me mad!So this works perfectly echoing characters via uart8:  int ch = 'A'; while (1) { HAL_UART_Transmit(&huart8, (uint8_t *)&ch, 1, 0xFFFF); HAL_UART_Receive(&huart8, (uint8_t *)&ch, 1, 0xFFFF); }  Now if I have getchar ...

ACapo.1 by Senior
  • 3413 Views
  • 4 replies
  • 4 kudos

Resolved! STM32F1 DFP problem

Keil MDK Device DatabaseIf no parameter, it needs to look like thisSo, MDK can not setting "Option for target-debug" correctly 

Shiina_1-1711786767072.png Shiina_3-1711787043912.png Shiina_2-1711786921695.png
Shiina by Associate III
  • 2286 Views
  • 1 replies
  • 0 kudos

STM32 Printf UART does not wait for transmission to complete

Hi, I am trying to implement printf with UART using DMA. The problem is when i use consecutive printf's in my code, transmission of the first data is not being waited. I implemented a control block to check if the transmission is completed but it doe...

ÇSerp.1 by Associate II
  • 3187 Views
  • 3 replies
  • 3 kudos