cancel
Showing results for 
Search instead for 
Did you mean: 

Forcing boot from FLASH from "a unique entry point in main Flash memory." ??

Tobe
Senior III

In the RM it says the above, but the only information i can find in the chapter that is referenced to is: "force boot from FLASH".

Is there a way to define a "unique" entry point, or ist this just wrong in the manual?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Perhaps it could be written better, but 0x08000000 is a unique entry point. You cannot boot to an arbitrary FLASH address on this chip. Some families such as the STM32H7 let you put a custom address to boot from.

If you feel a post has answered your question, please click "Accept as Solution".