STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Printf UART does not wait for transmission to complete

Hi, I am trying to implement printf with UART using DMA. The problem is when i use consecutive printf's in my code, transmission of the first data is not being waited. I implemented a control block to check if the transmission is completed but it doe...

ÇSerp.1 by Associate II
  • 3186 Views
  • 3 replies
  • 3 kudos

Resolved! 3.3V power supply for NucleoF103

Hello,I need to power the NucleoF103 development board using an external 3.3V power supply. I have read in the NucleoF103 manual that this is possible by removing SB2 (to disconnect the voltage regulator output) and SB12 (to disconnect NRST). I also ...

Resolved! Erasing memory corresponding to segment 0: Erasing internal memory sectors [0 150] Error: failed to erase memory

Hi. I am using STM32L010C6tx processor. I drew the circuit myself. I did SYS-> debug serial wire. I was able to install without any problem. But sometimes "Memory Programming...Opening and parsing file: ST-LINK_GDB_server_a14408.srec File : ST-LINK_G...

ZKURT.1 by Senior
  • 16324 Views
  • 10 replies
  • 0 kudos

Putting STM32L452 Sleep Mode

I'm developing a board with an STM32L452 and would like to find out if I can low the power consumption.The current draining is 35mA, my goal is lower it to 20mA or less to achieve a requirement.I've tried putting the device to sleep putting SLEEP MOD...

jkfc95 by Associate
  • 1034 Views
  • 1 replies
  • 0 kudos

How to connect the MIPI display with ST controller

Hi Team,We have an LCD with a MIPI display. We need to connect with the STM32 MCU.Please find the pin details on the LCD. We need to connect MIPI_0+, MIPI_1+, MIPI_2+, MIPI_3+, MIPI_4+,MIPI_0+, MIPI_1-,MIPI_2-, MIPI_3-, MIPI_4-.Kindly suggest ST cont...

SK22_0-1704367201554.png SK22_1-1704367266591.png
SK.22 by Associate II
  • 2842 Views
  • 4 replies
  • 1 kudos

COMP and blanking Function

Hi all,I am having some problems connecting a comparator to a TIMER using its blanking function (as described in the AN4232 application note).I've read the COMP_OutputBlanking example found in the STM32G4 repository projects (I'm using a STM32G431).I...

FlavioB by Associate II
  • 2103 Views
  • 2 replies
  • 0 kudos

Resolved! Pulses to KWh conversion in Energy meter

Hi,I am working with STM32G491RE.I communicating  ATM90E26 single phase energy meter with STM32 through SPI communication.I can able to read voltage ,current values correctly from the meter.For KWH calculation, I am reading Absolute active energy reg...

sireevenkat1_0-1712211776138.png

Resolved! FMC-SRAM Configuration for STM32F40G-EVAL

Hello there,   I am working on a project using an STM3240G-EVAL board which as the STM32407IGH6 MCU on it. In this project, I want to use USB-OTG-FS to connect an external USB microphone to the board and then store any information sent into the micro...

STM32H723ZG reading vref problem

Hello, i am trying to read internal temperature and vref values from ADC3. I shared ADC3 ioc settings. ADC clock mux freq is 96MHz and sampling time is set to ADC3_SAMPLETIME_247CYCLES_5.On init routine calibration line as below :HAL_ADCEx_Calibratio...

iocADc.PNG
Enes1 by Associate
  • 982 Views
  • 0 replies
  • 0 kudos