HelloI need to use full featured Teseo-Suite.Sending letters to st-teseo-suite-support@st.com remain unanswered.How could I obtain a full version of Teseo-Suite?Thanks
I'm having problems with USB on NUCLEO-U575ZI-Q (STM32U575).I've created from scratch project in CubeIDE for USB CDC ACM device, and set up all th peripherals as in the example STM32Cube_FW_U5_V1.4.0\Projects\NUCLEO-U575ZI-Q\Applications\USBX\Ux_Devi...
I've downloaded archive "en.STM32CubeExpansion_Crypto_v4.0.1.zip", now I'm trying to install it in STM32CubeMX with "From Local..." feature, but I'm getting error. How can I install the library in CubeMX?Thank you.
Hi @Peter BENSCH Thanks for quick response.Yes, I received avtivation key.I have folowing question: can I reuse same key on diferrent computers, or should I request a new key each time?
Hi AmelThanks for the reply.Yes, example project Ux_Device_CDC_ACM works perfect on my board.Ragerding heap and stack size, they are set to 0x200 for Minimum Heap Size and 0x400 for Minimum Stack Size, just as in example (if you mean stack an heap si...