STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 OSC Problem

Hi everyoneI'm currently using the NUCLEO-F429ZI development board. I'm planning to create a PCB using the STM32F429ZIT6, but I've encountered some questions during the planning stage.According to the datasheet, HSE_OSC is specified to provide 8MHz, ...

Scarlet by Associate III
  • 10599 Views
  • 20 replies
  • 16 kudos

Resolved! How to abort SPI Slave when Master requests for less bytes?

Hi,I have my master and slave applications running on NUCLEO-H563ZI Boards both of which normally receive/transmit  10 bytes of data in each SPI transfer. I use SPI in DMA mode.However, in one test case, master starts a SPI transaction for only 4 byt...

WCarey by Associate III
  • 3936 Views
  • 7 replies
  • 3 kudos

Losing data sending over USB CDC

Dear community,I am working with the STM32 Nucleo F429ZI board to send data over USB - CDC. I have set a time interrupt every 1ms and my goal is to send a package of data after each time interrupt (the data sent are consecutive numbers).As the code b...

alejandro_a_0-1689934743795.png

Hardware oversampling on ADC1 & 2 on H743VIT6

I'm trying to optimize the H743's hardware oversampling on ADC1 & 2 at 384KHz sampling rate, it reduces the noise but I'd like some advice on the settings.The H743 ref. manual state that the oversampling Ratio values are 0 - 1023, setting the number ...

Robmar by Senior III
  • 1112 Views
  • 0 replies
  • 0 kudos

Resolved! MB1549-U575ZIQ-C03 Board ,FDCAN don't work at FDCAN_MODE_NORMAL

board:MB1549-U575ZIQ-C03  (mcu stm32U575) I debug the FDCNA function with a CANalyst tool  1. Work at FDCAN_MODE_BUS_MONITORING mode, It can receive data from the CANalyst tool  2. Work at FDCAN_MODE_EXTERNAL_LOOPBACK,It can receive data itself and t...

dylanou by Associate III
  • 3360 Views
  • 8 replies
  • 0 kudos

Resolved! Multi ADC in parallel

Hi, I'm using  multi channels ADC3 of "STM32H735ZGT6" (3channels) I want to use these channels in parallel, but I've only found a way to convert in order in the Datasheet. Can I run all the ADC3's channels at once in parallel?If that is the case, can...

giwonKIM by Associate III
  • 1939 Views
  • 2 replies
  • 0 kudos

stm32 virtual com port on windows 11

I am working on stm32f439zi (nucleo) usb port with windows 11. After I enabled usb port functions on stm32cubeide, I got definition as followed for usb port:  when I connect device to windows 11 desktop. it looks like device use standard Microsoft us...

yanghong_0-1713462081776.png yanghong_1-1713462159422.png
yang hong by Associate III
  • 3827 Views
  • 1 replies
  • 0 kudos