STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Muxed FMC reference schematic

Hi,I'm working on a hardware design using the STM32F765VIH and I am trying to connect a MT28EW128ABA1HPC-0SIT NOR Flash and IS66WVH16M8DBLL-100B1LI PSRAM to the FMC in muxed mode. I'm struggling to understand how the muxed connection should be made a...

gosal by Associate III
  • 3733 Views
  • 5 replies
  • 0 kudos

ADC with DMA and 3 Channels

i'm trying to get a 3 channel dma up and running on my u5, but unfortunately i keep getting the error handler at line 122 that the a/d can't start via dma. do i need to do something additional here or not? i've already clicked through some posts and ...

Multiple channels used for TIM1

Hello,My final goal is to output two pulses from two separate pins, but not at the same time. My intention is to use TIM1 for my STM32F401RE board, as this is the only timer that allows me to set the repetition counter for the 'One Pulse Mode'. This ...

Kalle by Associate
  • 1201 Views
  • 1 replies
  • 0 kudos

Resolved! How to get free memory on USB drive with FatFs?

Hello,I would like to get free memory on USB drive (64GB, FAT32) with FatFs library. Here is part of my code:  DWORD fre_clust, fre_sect; uint64_t free_memory; res_file = f_mount(&fs, "0:", 1); res_file = f_getfree("0:", &fre_clust, &fs); fre_sect =...

Ondrej1 by Associate II
  • 1748 Views
  • 1 replies
  • 0 kudos

Resolved! [STM32L476RG] Jump to Bootloader from Software.

Posted on April 19, 2017 at 09:27 Hello, I want to use DFU for update my program on the STM32L476RG. I use a personnal board. When I put BOOT0 to VCC, the Bootloader start and we can change the firmware but my system is on battery and I have n...

Handling UART receive

I'm looking into creating a splashscreen and handling the uart responses. How can I wait for the input without consistently sending the response messaging. I'm unsure how to handle responses from the uart receive line.  enum splashscreen_response_typ...

mm.51 by Associate II
  • 1568 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer Error: No STM32 target found!

I have a STM32F405RGT6 on a custom PCB and are using a ST-Link/V2 ISOL in my computer. A USB-Mini is conencted to the ST-Link and from the ST-Link I use RESET, SWCLK, SWIO and GND to my STM32. I have tried connecting to the ST-Link with the STM32Cube...

mathieusteketee_1-1713515915240.png mathieusteketee_2-1713515989028.png mathieusteketee_0-1713515888552.png mathieusteketee_3-1713516411253.png

Resolved! STM32H750XBHX - CANFD Callback problem

Hey, I have a problem with the callback for FDCAN1. I am sending frames through ucandevices converter but the callback for FIFO0 is not called. The frames are definitely arriving, I added a test FreeRTOS and a task to receive and send frames to CAN1 ...

sqwerize by Associate III
  • 9916 Views
  • 16 replies
  • 4 kudos