cancel
Showing results for 
Search instead for 
Did you mean: 

Erase - unlock STM32L083

JR2963
Senior II

I am using STM32L083 and need to erase it using J-Link. If it is locked at Level1, I also need to unlock it. My goal is to completely erase the entire Flash memory. I believe I have an error in the process, as I have been unsuccessful in both erasing and unlocking. Could anyone please advise me?

Thank you very much, for any help.

My attempt:

 

 

 

 def eraseMCU(self):
                self.Jlink.connect(self._mcuToConnect, speed = self._swd_speed_khz)
                self.unlockFlash()
                self.unlockOptionBytesArea()
                self.programoptionBytes(RDP_UNLOCK) #0xAA
                self.reloadOptionBytes()
                self.Jlink.reset(ms = 1,halt = False)

 

 

 
where:
 
 

 

 

RDP_UNLOCK = 0xAA

PRGKEY1 = 0x8C9DAEBF
PRGKEY2 = 0x13141516
PEKEY1 = 0x89ABCDEF
PEKEY2 = 0x02030405
OPTKEY1 = 0xFBEAD9C8
OPTKEY2 = 0x24252627

PECR_LOCK_BIT =   (1<<0)
PECR_PRGLOCK_BIT = (1<<1)
PECR_OPTLOCK_BIT = (1<<2)
SR_EOP = (1<<1)
SR_BUSY = (1<<0)
OBL_LAUNCH = (1<<18)

FLASH_PECR = 0x40022000+0x4
FLASH_PEKEYR= 0x40022000+0x0C
FLASH_OPTKEYR = 0x40022000+0x14
FLASH_OPTR = 0x40022000+0x1C
FLASH_PRGKEYR = 0x40022000+0x10
FLASH_SR = 0x40022000+0x18


def unlockFlash(self):
        self.busy_wait()
        tmp = self.readU32Mem(FLASH_PECR)
        if (tmp & PECR_LOCK_BIT ) != 0:
            if self.writeU32ToMem(FLASH_PEKEYR,PEKEY1) == True:
                if self.writeU32ToMem(FLASH_PEKEYR,PEKEY2) == True:
                    return True
 
def unlockOptionBytesArea(self):
        self.busy_wait()
        tmp = self.readU32Mem(FLASH_PECR)
        if not tmp & PECR_LOCK_BIT:
            if tmp & PECR_OPTLOCK_BIT !=0 :
                if self.writeU32ToMem(FLASH_OPTKEYR,OPTKEY1) == True:
                    if self.writeU32ToMem(FLASH_OPTKEYR,OPTKEY2) == True:
                        return True
 
def programoptionBytes(self,val):
        val = self.option_bytes_word(val)
        self.writeU32ToMem(0x1FF80000,val)
        self.busy_wait()
 
        flash_sr = self.readU32Mem(FLASH_SR)
        if flash_sr & SR_EOP != 0:
            self.writeU32ToMem(FLASH_SR, SR_EOP)

def reloadOptionBytes(self):
      tmp = self.readU32Mem(FLASH_PECR)
      tmp |= OBL_LAUNCH
      print(hex(tmp))
      self.writeU32ToMem(FLASH_PECR,tmp)

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0