STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U031G8Y6TR Availability

The STM32U0 Series is very interesting, and I would like to use the small WLCSP package in a design for a new product, but the  STM32U031G8Y6 is still in evaluation. Does anyone know when the STM32U031G8Y6TR will be available for purchasing?Thank you...

vard by Associate II
  • 2561 Views
  • 4 replies
  • 0 kudos

The DMA impact of SPI on ETH in STM32H7

Hi All.In STM32H743, if ICache is enabled and DCache is turned off, SPI frequently uses DMA to transfer data(SPI transmission interval is within 10ms), and ETH may experience transmission lag; If ICache and DCache are turned off, there is no problem ...

ketlen_0-1707031085989.png ketlen_1-1707031103584.png ketlen_2-1707031243860.png
ketlen by Associate II
  • 1770 Views
  • 1 replies
  • 0 kudos

Chaining two timers on the STM32G4

I need to chain two timers together to get one 48-bit timer that counts microseconds, I'm thinking of using TIM2 as the master and TIM3 as the slave. I have the feeling some of the answers are contained in this table in the Reference Manual but I can...

c_shearer_cooper_0-1711461609158.png c_shearer_cooper_1-1711461683863.png c_shearer_cooper_2-1711461691949.png

SPI communication

Hello,I have problem with establishing wifi connection on STM32H7B3I-DK. I am using SPI2. I dont get any response. I am using simple AT command, that should give response 'OK'.  This is my int main() and initialisation of SPI2:int main(void){/* USER ...

Resolved! ADC doesn't work after code gneration

I’ve been working on a project for a while and initially generated the code only once at the beginning to set up the hardware configuration. Recently, I updated STM32CubeIDE from version 1.14.1 to 1.15.0. After updating, I regenerated the code withou...

Anassoumi by Associate III
  • 5762 Views
  • 9 replies
  • 1 kudos

Resolved! Identifying Silicon Revision of STM32H735IGK6U

Hello,we are using STM32H735G-DK Eval Boards equipped with differently marked STM32H735IGK6U chips.One saying:-------------------STM32H735IGK6UAA126   VQ ZTWN AA 109                    D2--------------------and the other one saying:------------------...

rk_iot by Associate III
  • 2311 Views
  • 2 replies
  • 0 kudos

Regarding RTC Alarm Interrupt

Hello STM32 Community,I'm currently working with the RTC peripheral on an STM32F4 device, and I have a question regarding RTC alarm events.I've been able to generate interrupts at specific intervals, such as 250ms or 500ms etc, using the RTC alarm fe...

san123 by Associate
  • 1742 Views
  • 1 replies
  • 0 kudos

Question about HSE and LSE

Hello guys. I'm trying to design a custom pcb that uses an STM32h7a3zit mcu and one of the most confusing parts is clock configuration. I will mainly use the hs usb interface. I've searched a couple of online sources and from what i could find is tha...

Στιγμιότυπο οθόνης (701).png Στιγμιότυπο οθόνης (700).png

STM32U5: UART Frame Error on High System Clock Speeds?

Greetings,I'm having a UART Frame Error (identified by relevant bit raised in UART ISR, and relevant error flag routine in UART_IRQHandler) when attempting to running LPUART1 off a 120MHz SysClock on a STM32U575RG present on our boards.I've replicate...

Tool recommendation for measuring load on STM32F072CBTx

Hello everyone,I hope you're all doing well!I just wanted to take a moment to express my gratitude for all the guidance and assistance I've received from this community. Thanks to your support, my learning journey with ST Microcontrollers, particular...

Ali5 by Associate III
  • 1501 Views
  • 2 replies
  • 0 kudos