cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5Ax USB issue

mpico
Associate II

I have a problem with USB initialization on those specific MCUs. Initialization function generated automatically by CubeMX hangs on USB_CoreReset function. Specifically on USB_OTG_GRSTCTL_CSRST bit which doesn't want to set after the reset. The Cube examples (which are working) use USBPD library only which source is not given so I can't see how initialization is done there.

With older USB32U5 where USB_FS phy is embedded everything works fine. Any ideas what should I change to make it working? My goal is to use it with tinyusb library since I don't want to use Azure RTOS or any RTOS in my project

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mpico
Associate II

Ok I solved that. It seems the problem is in SMPS my boards had included. If I switch it off everything works smooth. My guess is that HAL examples need more time to init the azure rtos and this small delay helps to solve this issue. Anyway USB works fine

View solution in original post

5 REPLIES 5
mpico
Associate II

Ok I solved that. It seems the problem is in SMPS my boards had included. If I switch it off everything works smooth. My guess is that HAL examples need more time to init the azure rtos and this small delay helps to solve this issue. Anyway USB works fine

waclawek.jan
Super User

Thanks for coming back with the solution. Please click on "Accept as solution" in your post so that the thread is marked as solved.

JW

I have also encountered the same problem, how to solve it!

liyang
Associate

I have also encountered the same problem, how to solve it!thank you very much for your help!

Where you put the delay?