STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer callback issue?

Hi,I have timer with period 1 sec (80 MHz clock):  htim2.Init.Prescaler = 80-1; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; htim2.Init.Period = 1000000-1;  Global var (volatile uint32_t) increased every time counter wraps around void HAL_TIM_PeriodE...

Lex by Associate III
  • 2048 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H503EBY uart bootloader

Hello! The AN2606 manual does not describe which pins of STM32H503EBY UART1 uses.STM32H503EBY have WLCS25 package, but i found information only for others packagesOn SO8, WLCSP18, TSSOP20, and UFQFN28 packages USART1 PA9/PA10 IOs areremapped on PA11/...

EAlek.3 by Associate
  • 1260 Views
  • 1 replies
  • 0 kudos

no indication on the display

Hello,what do I have to change in the code so that I see something on the oled display 0x78?Maybe someone has a tip for meThanks :)...#define ssd1306_I2C_Port hi2c2#define ssd1306_I2C_ADDR 0x78...#define ssd1306_WIDTH 128#define ssd1306_HEIGHT 64...I...

SPI_Receiving data is improper because of HAL Functions

I am sending multiple bytes in spi protocol. The sender is sending properly through AARDWARK(Total Phase Control)Software. But only the odd number of bytes are received and the receiving is not proper using these HAL_Functions. What is the issue?int ...

Resolved! SPI_multiple_bytes_transfer

I am sending multiple bytes in spi protocol. The sender is sending properly through AARDWARK(Total Phase Control)Software. But only the odd number of bytes are received and the receiving is not proper using these HAL_Functions. What is the issue?chec...

Resolved! STM32G474VET3: DAC output and comparator input question

As i am using inside comparators. For that i can see below available options for reference voltages. My question is about DAC output can it be set internally or i have to make physical connection by DAC out put pin to comparator input  

sag_0-1714040226057.png
sag by Associate III
  • 2055 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Nucelo F429ZI, LWIP a simple application not working

Hello everyone,  I have been trying to run a simple LWIP application on my STM32 F429ZI board. I can see the LED green and orange of the Ethernet jack (CN14) are on which indicates the link is up and running. but no luck with pinging the board from m...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.