User Activity

Hello,Is there a way to get schematic reviewed without sharing it publicly? My company doesn't allow public posts, so wondering if there is any possibility private reviews. Thank you!
Hello,I had order 2x STLINK-V3MINIE and one of them has CLK and GND shorted. Looking for suggestions on what needs to be done since it has happened out of the box when I opened fresh one.Thank you!
Hello, I'm planning to use 4xSTSPIN32F0 on one PCB and I was planning to use one input supply(3.3V, 1.5A) for all 4xSTSPIN32F0. I'm struggling to understand power architecture of STSPIN32F0 when using 3.3V supply. Does it need separate 12V at VREG12V...
Hello, I don't know whether this is appropriate place to ask, But will STM32H7A3RIT6 or H7B3RIT6 a good choice for projects considering availability? Are these in production to use on new products and trust the availability exists? Thank you! 
Hello,I'm trying to program G491KCU6 board via UART1 and I'm not able to connect to st-programmer. I don't know whether the board is actually entering Boot0 or not. I have PB8 with 10K to GND and I pull it up during connection to enter Boot0. Below i...
Kudos from
Kudos given to