STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 ADC4 unable to set AUTOFF bit

I am unable to switch on the AUTOFF bit in ADC4.DS reads about ADC_PWRR/AUTOFF: The software is allowed to write this bit only when ADEN bit is cleared to 0 (this ensures that no conversion is ongoing).But if this bit is set, the ADC doesn't set ADRD...

Sleep stop standby mode - when to use them

Hi i m currently coding standby mode to conserve battery energy a application, i know its the lowest current consumption, what and when to use the 3 modes? which mode should i use if i wana save battery life yet i still want SPI DMA to transfer in th...

STM32F446ZEJ6 Daisy Chain JTAG

Hello,I am currently working on a project where we have daisy chained the 5 Pin JTAG of STM32F446ZEJ6 with a TI microprocessor AM24x series. My question is that is there a way I can get a configuration file for the STM32 to create a new custom config...

PLC Likes ON-PULS

I would like to generate a pulse by timer.Idle state: GPIO-PIN HIGHafter internal trigger: GPIO-PIN LOWafter 1us  back to GPIO-PIN HIGHi have try by PWM, OC  and one pulse enabled mode.but my pulse is starting after 1 us.

nimaltd by Senior
  • 1171 Views
  • 1 replies
  • 0 kudos

Migrate from STM32F401CCUx to STM32F103C8T6

I've done a long search on the Internet but only found the migrated STM32F103 to the STM32F4 series, not vice-versa. So I'm asking anyone who can help me. To be specific I am going to try this project from GitHub but in my case, I'm going to use STM3...

Resolved! STM32H5 SWO debugging

Hi, We want to use now the STM32H5 for future projects. In the past, we used STM32F4 with enabled SWO for debugging. Is there any example available to get this feature working for STM32H503? Would be great to do it on register level to be independent...

AnRe by Associate II
  • 7842 Views
  • 8 replies
  • 2 kudos

Flash Memory

We are using STM32F373VCT6 Microcontroller for our application and we want to use an External Flash Memory of 1MB with this controller. Can you suggest some NAND/NOR Flash memory of 1MB, that supports SPI/QSPI and is compatible with this controller a...

Revathi by Associate
  • 5790 Views
  • 2 replies
  • 2 kudos