STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Warning on passing argument

Hi everybody,I have a lot of the same warnings, but the compilation is ok! I would still like to try to solve themin my main.c in this line : st7567_Write_Number2(100, 27, D_seconde, Number_microsoftSansSerif_14pt, INFO_Number_microsoftSansSerif_14pt...

JJoao.1 by Associate III
  • 1021 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G0 Uart Prescaler

I work on a project with the STM32G0 and one difference between the F0 series is, that the UART has a clock prescaler. The maximum UART peripheral clock (usart_ker_ck) is 64 MHz (max of SYSCLK and PCLK) and this clock can be prescaled with PRESC -> u...

Resolved! STM32H7 and PDM2PCM filter (for PDM microphones)

I have some questions and remarks about the PDMFilter (used for PDM MICs).I have it working fine on a Portenta H7. Almost all OK.I have studied the UM2372 : STM32Cube PDM2PCM software library for the STM32F4/F7/H7 Series - User manualHere are my ques...

PDMFilter_1a.png PDMFilter_1b.png PDMFilter_1c.png
tjaekel by Lead
  • 3618 Views
  • 2 replies
  • 0 kudos

STM32F407: PLL is not working

I have build a code of Mcu driver for STM32F407 DISCOVERY board. During Flashing my HSE or HSI works fine but PLL doesn't works on. I will attach the the mcu.c and mai.c file for your reference. Kindly have a look into this help me out.

Resolved! Optimization causes "No open pipes!" STM32H723ZGT6

This is on a STM32H723ZGT6 Ok for testing i went to a blank project with only the usb turned on. Set asUSB OTG HSDEVICE ONLYHIDUsing the defaults for everything. With no optimization it works and shows up correctly. With any kind of optimization turn...

Resolved! STM32G474RE General purpose timer (TIM16)

Greetings,I am trying to set TIM16 on 1us period but the smallest period I am able to achieve is 4us here is the values of my prescaler and auto-reload register(ARR). I am working with the HAL.SysClk = 170MHzPSC = 16 (+1 will be added) ARR = 9 (+1 wi...

Vueko by Associate III
  • 1648 Views
  • 1 replies
  • 2 kudos

Soft error handling for Flash on STM32G473

Hi. I am working with STM32G473 for a safety application. I cant find a reference to how the soft errors are handled by the MCU especially for the flash. Also where could I find Soft error rates for this particular MCU? Thanks.

SMahm.2 by Associate II
  • 839 Views
  • 0 replies
  • 0 kudos