STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need a driver for USB to CAN for Windows 11 Arm

Hi I am new here. I am looking for a driver for Windows 11 Arm (parallels M1). The chip on my board says STM32F105. The driver that worked for me last time on other Windows was:  dpinst_amd64 Can someone advise a driver for Windows 11 Arm (running Pa...

grisom by Associate II
  • 8737 Views
  • 10 replies
  • 6 kudos

CPU Utilisation in STM32

Hi How Do I get the cpu utilisation in stm32?I am using STM32F205 with platformIO Ide.I dont want to use Task list view in freertos as it is intended for debugging only.Any help would be much appreciated.Thanks

JThom.15 by Associate III
  • 1254 Views
  • 1 replies
  • 0 kudos

unable to get the output from the code:

Hi Community.I am Running a code which takes two adc values to generate duty  and one timer for PWM generation. Elaborately i am running an MPPT code by taking voltage and current from PV panel which is read by PA0 and PA1 of STM32F446re micro contro...

STM32U5G9-DK2 - Power the board using external 5V

Hi, looking at the scheme it seems possible to power the board by providing an external 5V supply on the 5V Arduino PIN (CN5, pin 5, which is the output of the linear regulator feeded by V_IN), and removing all the jumpers on the CN1. Is it correct? ...

bluluiss by Associate II
  • 1706 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 cryptographic firmware library for STM32U5

Hey,in the past we used a STM32F4 and in the new Gen I will use the a STM32U5 and there is my questen about the cryptographic firmware in the past we could use the libSTM32CryptographicV3.0.0_CM4_GCC.a but now is there also a Lib for the stm32u5? 

Resolved! Timer's Combined Channels - Encoder Mode

Hello, I'm using the nucleo-h743zi2 board.When obtaining the value of TIM2->CNT (or TIM5->CNT) through the combined channels of TIM2 or TIM5 on this board, without any special settings, I can perceive the encoder rotating in reverse as a negative val...

HMsDobby2 by Associate III
  • 2285 Views
  • 1 replies
  • 1 kudos

STM32F407 Measuring tie between 2 impulses

Hey. I am working on a task which requires to measure time between 2 different impulses with high precision. We have custom board that generates output pulse based on the capacitor and resistor values. The Input is LOW to HIGH impulse (Green color on...

LPetr1_0-1714725999122.png LPetr1_2-1714723304279.png LPetr1_1-1714723277892.png LPetr1_3-1714723402569.png
LPetr.1 by Senior II
  • 6553 Views
  • 9 replies
  • 1 kudos