cancel
Showing results for 
Search instead for 
Did you mean: 

MCU State changed or unchanged when waking up from stop mode

HDaji.1
Senior

I am using F411 as the main controller of some DAC/ADC modules.

I need to put MCU in stop mode to reduce its power consumption.

I wonder whether or not I need to configure all the I2C, SPI, and UART interfaces when MCU wakes up from stop mode.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

Hello @HDaji.1 

When the STM32F411 MCU wakes up from stop mode, it's necessary to reconfigure the clock.

the need to reconfigure all the I2C, SPI, and UART depends on your specific configuration, if these interfaces are disabled or their configuration is altered during stop mode, you will need to reconfigure them upon wakeup. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Sarra.S
ST Employee

Hello @HDaji.1 

When the STM32F411 MCU wakes up from stop mode, it's necessary to reconfigure the clock.

the need to reconfigure all the I2C, SPI, and UART depends on your specific configuration, if these interfaces are disabled or their configuration is altered during stop mode, you will need to reconfigure them upon wakeup. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

HDaji.1
Senior

thx, @Sarra.S 

I saw a sample code, which uses RTC to wake up MCU:

  HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
  HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
  SystemClock_Config();
  HAL_ResumeTick();

 As you said, the 3rd line is to configure clock.

I have 3 more questions to trouble you:

  1. What does HAL_ResumeTick do?
  2. If I want to reduce power consumption as much as possible, before MCU goes to stop mode, is it better to disable I2C, SPI, and UART?
  3. I don't understand why their configuration can be changed during stop mode. Could you give an example?
Sarra.S
ST Employee

>>What does HAL_ResumeTick do?The HAL_ResumeTick function is used to resume the SysTick interrupt, which is often disabled during low-power modes to prevent it from waking up the CPU every 1ms

>>If I want to reduce power consumption as much as possible before MCU goes to stop mode, is it better to disable I2C, SPI, and UART?

these peripherals can draw power even when they're not actively being used, so yes, it's better to disable them

>>I don't understand why their configuration can be changed during stop mode. Could you give an example?

some peripherals may have settings that are designed to change during low-power modes to further reduce power consumption. An example could be a peripheral that has a low-power mode of its own, which is automatically enabled when the MCU enters stop mode. This is not necessarily applicable in your case 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.