cancel
Showing results for 
Search instead for 
Did you mean: 

STM32l4 + tinyusb + msc + sdmmc

NW.2
Associate II

Hi!

 

I'm currently trying to mount my sdcard via MSC/SDMMC and tinyUSB. It worked fine with RAM, could read and write, but I probably do the commands wrong for SD Card. Mounting with FatFS works fine, but I cannot get it to display any device on my drive. It just shows the SD Card and wants to format it, which will always fail.

 

Here are the functions I use for MSC, just changed the fufnctions from RAM readings to SD Card readings.

 

 

 

 

int32_t tud_msc_write10_cb(uint8_t lun, uint32_t lba, uint32_t offset, uint8_t* buffer, uint32_t bufsize)
{
  (void) lun;
//  if ( lba >= DISK_BLOCK_NUM ) return -1;
//    size_t addr = lba * BLOCK_SIZE + offset;
    HAL_SD_WriteBlocks(&hsd, (uint8_t*)buffer, lba, bufsize, 10);

//  while (HAL_SD_GetCardState(&hsd) != HAL_SD_CARD_TRANSFER){}


  /* Wait until SD card is ready to use for new operation */


  return (int32_t) bufsize;
}

int32_t tud_msc_read10_cb(uint8_t lun, uint32_t lba, uint32_t offset, void* buffer, uint32_t bufsize)
{
  (void) lun;

  // out of ramdisk

//  uint8_t const* addr = msc_disk[lba] + offset;
//  size_t addr = lba * BLOCK_SIZE + offset;

// HAL_SD_ReadBlocks(&hsd, buffer, addr, bufsize, 100);
  HAL_SD_ReadBlocks(&hsd, (uint8_t*)buffer, lba, bufsize, 10);

 /* Wait until SD card is ready to use for new operation */
// while (HAL_SD_GetCardState(&hsd) != HAL_SD_CARD_TRANSFER){}


  return (int32_t) bufsize;
}

void tud_msc_capacity_cb(uint8_t lun, uint32_t* block_count, uint16_t* block_size)
{
	  HAL_SD_CardInfoTypeDef info;
	  HAL_SD_GetCardInfo(&hsd, &info);
	  *block_count =  info.LogBlockNbr  - 1;
	  *block_size = info.LogBlockSize;
}

 

 

 

 

 If anyone could tell me what I'm doing wrong, that would be so great, as I don't get any proper results with it!


Kind regards

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0