cancel
Showing results for 
Search instead for 
Did you mean: 

DMA request generation on STM32H7

HansPLJ
Associate III

Hi!

I am looking into the possibility on using LPTIM1 to trigger a DMA transfer with no CPU interrupt. This timer is chosen because it can be clocked directly by the HSE clock input. In the datasheet of STM32H7B3 (DS13139 - Rev 8) table 4, it states that LPTIM1 cannot be used for DMA request generation. In table 103 in the reference manual (RM0455 Rev 11) lptim1_out is listed as as a resource. 

Does this mean that it is not possible to use an output from LPTIM1 directly as an DMA request generator, but it is possible when using the DMA mux?

Any clarification would be appreciated! 

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hello @HansPLJ 

It is not possible to use directly DMA request generation. However, you can use it through DMAMUX. Your interpretation is correct.  By using a DMAMUX, you can dynamically switch the DMA channels source based on your system's requirements at any given time. This allows for more efficient use of the available DMA channels and greater flexibility in your system design.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

4 REPLIES 4
LCE
Principal II

I don't know that H7 / LPTIM. Check the LPTIM CR / IE registers, is there any "DMA enable" bit?

FBL
ST Employee

Hello @HansPLJ 

It is not possible to use directly DMA request generation. However, you can use it through DMAMUX. Your interpretation is correct.  By using a DMAMUX, you can dynamically switch the DMA channels source based on your system's requirements at any given time. This allows for more efficient use of the available DMA channels and greater flexibility in your system design.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
HansPLJ
Associate III

Thank you for the clarification! 

mƎALLEm
ST Employee

Refer also to the AN5224 "STM32 DMAMUX: the DMA request router"

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.