STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747 and I2C bootloader

Hello,I'm designing an electronic board with STM32H747 microcontroller. This is my first time using a microcontroller with 2 cores.I would like to ask some questions about bootloaders:- how do I select bootloader over I2C (I2C1 on PB6/PB9 pins)?- at ...

SSerg.4 by Associate III
  • 5044 Views
  • 2 replies
  • 0 kudos

Debouncing using registers

Hello, first of all, thanks for all the previous help to everyone. I want to debounce my input, using registers, but I'm running into the issue of it "not working" I am surely missing something in the logic I am overlooking.here is my interruptvoid I...

Petrarka by Associate II
  • 4220 Views
  • 1 replies
  • 0 kudos

unable to flash NUCLEO-H7A3ZI-Q

Hi Team,we are facing issue with flashing NUCLEO-H7A3ZI-Q board.is any problem if we flash stm32h7a3zit6 code on stm32h7a3zit6q.can we give a suggestion ASAP

Resolved! USB configuration

Hi, I need to use USB in 2 modes:1. See SD card files interfaced to controller through computer via USB2. Transfer SD card files to "data storage device (USB stick)" via USBAny examples for same? Display menu should handle above operations. Since the...

GauravK by Senior
  • 1634 Views
  • 3 replies
  • 0 kudos

Resolved! SPI on STM32U575 (NUCLEO board)

I'm trying to get SPI1 working on an STM32U575 (NUCLEO board), starting from a base of existing working STM32F4 LL API code, but have failed.I am running this on a NUCLEO-U575ZI-Q board, so MOSI on PA7 (D11), MISO on PA6 (D12), SCLK on PA5(D13) and w...