STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Memory writing problem of STM32L452RE

Hello fellow seniors:I am still in the learning stage and currently use the part of writing to the memory (Flash Memory). I have encountered a problem and would like to ask for advice:From the picture (instruction manual) of [[Figure 1]], we can see ...

螢幕擷取畫面 2024-05-08 163233.png

STM32H747 (Portenta H7) and HardFault Crash Report

My project crashes after a random period when sending network traffic (one hour or longer working). I want to debug (but without a debugger connected or sitting there and waiting). So, I want to record some data, e.g. when the HardFault_Handler was c...

tjaekel by Lead
  • 1507 Views
  • 0 replies
  • 0 kudos

STM32F429II LTDC Image size error

Hello, I was controlling the LTDC image with STM32F429II (Flash 2MB, RAM 256 + 4KB) from ST.I think there is an error in memory allocation, so I leave a question.The compiler i use is IAR.Currently, we have implemented the RGB888 image as 1.22MB size...

Jdogk_0-1715230831448.png
Jdogk by Associate III
  • 1004 Views
  • 0 replies
  • 0 kudos

stm32 spin eval 3201 connection issue

After downloading the latest version of MC workbench required drivers and the latest firmware. I am still getting the following error in the IDE- "Connection Failed! No response, check communication cable, the power or the baudrate(set to 9600)". Ple...

Jayadeep by Associate
  • 623 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F401RE Pushbutton interrupt

So here's the code ; The issue with it is that whenever I press the button, weird things occur, such as my output resetting completely-going to the maximum, at my output I have a variable PWM signal void PB_Init(void){ RCC->AHB1ENR |= RCC_AHB1ENR_...

Petrarka by Associate II
  • 1929 Views
  • 3 replies
  • 0 kudos

Resolved! STMG431 RBT6 - ADC sync does not seem to work as per manual

Hi,i am testing the ADC at the moment, and the values i get out of it look pretty good. Except, when using a squarewave.See my video: https://www.youtube.com/watch?v=TmKADM2yQvU The manual states for having the ADC run from AHB clock: "... has the ad...

Tobe by Senior III
  • 3041 Views
  • 2 replies
  • 0 kudos

ADC DMA pointer issues

Hello everyone,First of all, I want to say that I have a very limited knowledge about C memory stuff, so a bit of guidance would be of help. I am trying to set up a timer-triggered multi channel ADC with DMA, which I have already succesfully achieved...

dweggg by Associate
  • 980 Views
  • 0 replies
  • 0 kudos

Resolved! Can COMP7\ETR1 reset TIM20 on only one edge instead of both?

I have TIM20 configured in reset mode and I want the output of COMP7 to reset it. I have TIM20 configured with ETR routed to COMP7 and I can see the timer being reset on both of the edges of the COMP7 signal. I only want TIM20 reset on one edge. I'm ...

KHarb.1 by Senior II
  • 1874 Views
  • 2 replies
  • 0 kudos