User Activity

Good morning,We designed a LED controller with the STM32C011. We exposed the BOOT0 PIN in our design as followed: Now the first prototypes are potted in without access to the SWD interface and we want to update the firmware via the internal bootloade...
Hello,Currently I'm playing around with the I3C peripheral and I try to implement a sort of "eeprom" interface on a I3C target where I have 10 slots which I want to be able to address separately.So on the controller side I have this function:  int i3...
Hello,I'm trying to implement an I3C target device which sends inband interrupts when I push the blue Nucleo button.But I also want it to be ready to receive data via a private message.To do this I call `HAL_I3C_Tgt_Receive_IT` after receiving a dyna...
Hi All,Today I received two NUCLEO-H503RB boards, but when trying to get the ADC calibration values the processor HardFaults. According to the datasheet it's the correct address: Also when trying to access it with the debugger it failsAlso the temper...
Currently I write locked the first few sectors of my STM32U575xx. However I would also like the unlock the write protection. Since both J-Link and the ST-Link cannot do this I thought about writing a small application and run it from RAM to reset the...
Kudos from
Kudos given to