STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Simple UART problem STM32H753

Hi,I'm relatively new to the STM32 world and I'm becoming frustrated that I can't make a simple UART work. No DMA, no interrupts just trying to send bytes out of the UART and then receive them. Here is my setup code:      void UART7_Init(void) { GP...

GlennH by Associate III
  • 6264 Views
  • 12 replies
  • 5 kudos

SPI lower harmonics problem with XPT2046 touch sensor

I had EMI problems interfacing with my 4.0" ILI9488 v1.1 display over SPI. Having a long cable (about 30cm) display and touch works when powered using ST-Link V2, but when i powered it using a generic 24V PSU, the display and touch is not working all...

Selecting RTC Internal wakeup line

Hi everyone!I have an u585 related question:Can I configure RTC internal wakeup line other than PWR_WAKEUP_PIN7_HIGH_3 ?In all u5xx examples used this line, but We have an external wakeup source on  PB.15.I can't change it in CubeMX and I can't find ...

ccuebler by Associate III
  • 2962 Views
  • 5 replies
  • 0 kudos

STM32G474 default option bytes configuration

Hello,I've another observation, may be something wrong in board.host controller is sTM32H573 which will update firmware of slave controllers interfaced on SPI one is sTM32G071 and is STM32G474, I'm using nucleo-g474re boardfor sTM32g474 controller sy...

0693W000006FmJtQAK.png 0693W000006FmKNQA0.png 0693W000006FmKhQAK.jpg
AShel.1 by Associate III
  • 5658 Views
  • 3 replies
  • 2 kudos

Resolved! STM32C011F6U6TR Boot Mode Selection Problem

Hello, I will use STM32C011F6U6TR in a project.Since I need to program with USART, I think I need to use the "boot from system memory" mode in BOOT mode, am I right?As written on the datasheet, there are 3 modes. When switching between these modes on...

How to trigger input capture

Hello All,I want to trigger an input capture when another timer overflows. I have both timers set up, but I am missing on how to make the overflow event trigger the input capture of the other timer. The reference manual has been a good help, but I ca...

Banana123 by Associate II
  • 4021 Views
  • 6 replies
  • 4 kudos

TSC peripheral - Linear Slider

Hello,I have a board with a interlaced 4 segment capacitive slider, not half-ended, connected to channels G2-IO2, G3-IO2, G4-I02 and G5-IO2, so in the same bank but different groups, as it should be I suppose. Can anyone please tell me what comfigura...

Resolved! stm32h747i-DISCO display issues

I recently bought an stm32h747i-DISCO and tried to run 2 example projects the "JPEG_DecodingFromFLASH_DMA" and the "JPEG_MJPEG_VideoDecoding". Both of them run correctly on M7 processor, but it seems the display has an hardware problem because it tur...

AFato.3 by Associate II
  • 3576 Views
  • 3 replies
  • 1 kudos