STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer interrupt discontinuity issue using stm32f103c8t6

Hi I am trying to generate interrupt every 100uSec using Timer-2 using stm32f103c8t6 blue pill. I have simply set the system clock to 72 MHz pre scaled the timer two by 72 time using 72-1 and setting counter period to 100. I have also enabled TIM2 Gl...

a.PNG b.PNG 1.jpeg 2.jpeg
Shahid by Associate II
  • 3172 Views
  • 5 replies
  • 0 kudos

Resolved! DMA SPI RX not receiving data

STM32G071R8 & M95160-WMN6TP EEPROMWe have the DMA SPI TX direction working but are having issues with the data that is being returned. Technically this is a read from the EEPROM but the command and read address are sent first. The EEPROM responds wit...

Capture.JPG Capture.JPG

Resolved! How does VREFBUF HIZ bit get set via CUBEIDE?

I have a project where VREFBUF outputs 2.0xxV correctly without intervention. I created a new project and I see VREFBUF output stuck at 0V, and I'm not sure what's causing the changed behavior.  I inspected the VREFBUF_CSR register and I see ENVR=1 a...

KHarb.1 by Senior II
  • 1696 Views
  • 4 replies
  • 0 kudos

Resolved! Zephyr MCUboot for Stm32

Using following settings:IDE : VS Code Programmer : Stm32Cube programmerStlink Debugger OS: Zephyr MCU: Stm32u5 series  I'm trying to use following link in order to sign application image: https://docs.zephyrproject.org/2.7.5/guides/west/sign.htmlIt ...

A Maq by Senior
  • 4150 Views
  • 2 replies
  • 2 kudos

Delay in SPI Transfer with STM32H7

Dear ForumIm using STM32 H755 ZI in the starter kit. I set the Timer 4 for generate a Interrupt each 1ms.At begin of INT:     -I toggle a PIN,      -and, send a SPI data (8 byte or 16..not important)What I noted is a delay of almost 10uS beetwen pin ...

Roibert by Associate II
  • 6448 Views
  • 13 replies
  • 3 kudos

I2C master transmission with DMA not Working

Hi I'm trying to establish a communication using I2C with a MCP45HVX1 digital potentiometer device with the stm32g474-re discovery board, I'm using I2C2 module that has been configured with MX with interrupt enabled. I'm using PF0 as SDA and PC4 as S...

Vueko by Associate III
  • 2235 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H7 playback example

Is there an application or example about an "audio playback" project using the SAI interface (SAIA-SAIB) connected to a Codec ?I'm using the Nucleo NUH723ZG board. Thank you, Carlo

carloV by Associate III
  • 1569 Views
  • 1 replies
  • 0 kudos

Resolved! Hello, I am trying to set up a FDCAN communication (STD Id) at a baud rate of 250 kbit/s in STM32G473RBT . The Tx part seems to work perfectly but I have a problem at the level of the reception.

I try to just toggle a led for each received frame (STD ID).With a logic analyser I checked the Rx pin on the Rx MCU and the frames arrive well. Hence my feeling that the problem lies at the level of the callback function where the MCU never go.Than...