User Activity

Hii I am using STM32F103C8T6 controller. In this controller I am using the UART1 and UART2 transmitting and receiving data. In UART1 I adjust 9600 Baud rate, 8-data bits, None parity and 1 stop in these configuration I am transmitting and receiving d...
Hii I am using STM32F103C8T6 controller and i want to initialize UART 7-Bit mode as per this configurations none Partiy Bit and 1 stop Bit. But in the controller has  these two parameters UART_WORDLENGTH_8B & UART_WORDLENGTH_9B. Then how to init UART...
I am using stm32f103rct6 controller board. I am not getting fixed ADC values for POT. I was used poll for conversion in ADC. Please attach code to get a fixed ADC value or else please address me for how to solve the problem.