STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IBIS model Configuration STM32U5A9

Greetings,   I have a question regarding the IBIS model of STM32U5A9 family. in the setup of any pin there is model parameter that has to be selected. There are several models such as io100m_ls_xx_xxx. what exactly those models mean in terms of actua...

Au by Associate
  • 1313 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 QUADSPI clock configuration

I have question about STM32H7 QUADSPI clock configuration.It seems STM32H7 contains two different source clocks.If I select HCLK3 as the clock source for the QUADSPI Clock Mux, how is the QUADSPI clock frequency calculated? Regardless of selecting HC...

nonoriri_0-1718245025308.png nonoriri_1-1718245090453.png
nonoriri by Associate III
  • 3347 Views
  • 3 replies
  • 2 kudos

Resolved! Switching between UART to GPIO and GPIO to UART

Hi     i am configuration UART1 as default and Tx pin switching into GPIO then  reset (Low) the GPIO for 28 micro sec(delay)  and set(high) the GPIO then again switching to UART1. during switching waveform level  is intermediate as show in below. (my...

Naresh_ by Associate III
  • 3778 Views
  • 4 replies
  • 3 kudos

STM32U5 Nucleo where to find demo source code

Hi community people, As an introduction, please note I'm completely new to the STM32 world, and back in embedded world after a long break in the application level. I now jump in a new project that will be based on a STM32U5, and I start digging in do...

PatriceL by Associate III
  • 3633 Views
  • 5 replies
  • 0 kudos

Resolved! Tying SPI inputs together to run several ADCs at once

Dear Community,I'm working on STM32H743ZIT6 based project.Here I want to set up 4 ADCs which have SPI interface.On developer's forum is said "If all ADCs will be sampled at the same point in time with the same settings, then the SCLK, CS, and SDI can...

Ajaho by Associate III
  • 8760 Views
  • 18 replies
  • 5 kudos

stm32 response transmission fault

i am using a stm32f401ccu6 board to receive modbus rtu requests from a master device(windows laptop running simplymodbus) and prepare the response buffer and send itso far i can see that the response buffer is being prepared as expected in the live e...

shiroval by Associate
  • 1263 Views
  • 0 replies
  • 0 kudos