Skip to main content
Associate II
March 19, 2024
Question

how to interface lvds 1920*720

  • March 19, 2024
  • 0 replies
  • 1188 views

DSI2HDMI display converter - SL-MIPI-LVDS-HDMI-CNV (somlabs.com)

how can i interface lvds display of 10.3 inch 1920*720 resolution with stm32f769-disc0 board.,,is there above module can be used for lvds signaling..or should i do schematic for interface board like below image which is done for eva board..my display is innolux DJ103IA-03B.

I WILLBE THANKFULL IF ANYONE CLEARLY EXPLAIN, as this is important for our dedicated HW too.
regards
embed_engr 

This topic has been closed for replies.