STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446RET6 Nokia5110

I am using CMSIS for STM32F446RET6 (clock speed at 180 MHz) to drive Nokia5110 LCD Module via SPI1. But, this program doesn't work. When I test with STM32F103C8T6 (using CMSIS and Clock speed 72 MHz), Nokia5110 work well. Please help me. How to corre...

May by Associate
  • 1296 Views
  • 2 replies
  • 0 kudos

ADC Conversion time of STM32U5A5

Hello,i've implemented a routine to measure some ADC channels with the MCU STM32U5A5ZJ.After one measurement is finished (interrupt triggers after conversion) i start the conversion for the next channel.Settings:ADC conversion: Single conversion mode...

Shaheen by Associate II
  • 2265 Views
  • 3 replies
  • 0 kudos

Resolved! Wrong message ID sent on FDCAN

I am using the FDCAN module on STM32H753 to send messages. The message ID is always the same: 0x7DF. So I create a static Tx header:  static FDCAN_TxHeaderTypeDef txHeader = { .Identifier = 0x07DF, .IdType = FDCAN_STANDARD_ID, .TxFrameType = FDCAN_DA...

MZadn.1 by Associate II
  • 3367 Views
  • 5 replies
  • 2 kudos

Issue to generate an alarm interupt on STM32C031

Hi,I try to configure a STM32C031K6 to generate an interupt every seconds using RTC Alarm A (RTC clocked by 32.768KHz crystal).I am working on STM32Cube IDE 1.15.1. First issue was that the device configuration tool does not generate any code regardi...

mjacquin_0-1718371573119.png mjacquin_1-1718371641930.png
mjacquin by Associate
  • 1125 Views
  • 0 replies
  • 0 kudos

STM32CubeMX Mac updater does not work

Hi,whenever I try to run the CubeMX updater on MacOS, using sudo, the update will fail with:" Updater cannot write on Software Folder. It's probably due to a bad Acces Privilege."I tried to give everyone, admin and me the right to read and write the ...

Resolved! Cannot get One-Pulse mode working

I know this might be a pretty basic thing to have issues with, but after banging my head against the wall on this for days, your snark-free assistance would be greatly appreciated.I am using a B-L072Z-LRWAN1 and trying to get timer 2 channel 1 to pro...

Resolved! NUCLEO-H563ZI_OEMiROT_Boot Example

Hi,I'm trying to integrate MCUBoot into an existing STM32CubeIDE project. As I wasn't sure where to start, I've found an example in STM32CubeIDE for NUCLEO-H563ZI.After generating the project, I've tried building it but I've got errors related to mis...

mjurjevic by Associate II
  • 5226 Views
  • 8 replies
  • 3 kudos