STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with DMA and USART receiving problem

Hello,I have an STM32F107 microcontroller that uses DMA and USART to receive 250 bytes every 10 ms. The RTOS tick is 1 kHz, so osDelay(1) results in a delay of about 1 ms.The sender transmits 200 bytes every 5 ms, and during this phase, it is not cri...

Resolved! UART sending some else data and not as intended

i am using STM3210e-eval board which has stm32f103zgt6 MCU no i am just sending data over uart to my pc the uart is interfaced with rs232 port so for the looking at the schematics i have connected it's tx and rx to ft232rl's rx and tx respectively an...

rahul7515 by Associate III
  • 6075 Views
  • 12 replies
  • 3 kudos

ADC Noise

We use a STM32F7xx microcontroller with LQFP144 casePart of the ADC Pins are on the 1-36 pin side.Unfortunately this is also the side where the Quartz (Pins  OSC_IN and OUT, PC14-OSC32_IN, PC15-OSC32_OUT) and the RMII_CLK are mapped.This leads to add...

gviereck_0-1699875868312.png
gviereck by Associate II
  • 8809 Views
  • 10 replies
  • 1 kudos

Resolved! STM32H750 About Dual-Flash mode program in QSPI

Hello,I may have a misunderstanding about Dual-Flash programming, so my question might seem strange.In Dual-Flash mode, does the write speed double?If so, I think the following code cannot achieve double the write speed in Dual-Flash mode. (stm32h7xx...

nonoriri by Associate III
  • 2195 Views
  • 3 replies
  • 2 kudos

Resolved! Getting started with STM32H753I-EVAL2

Hello,I would like to evaluate the STM32H753XI MCU and I suppose the right board for that is the STM32H753I-EVAL2. Since I am completely new to STM MCUs and MPUs, I would like to know a little about it:- Is it sufficient to have the board itself and ...

rbedin by Associate II
  • 3571 Views
  • 5 replies
  • 5 kudos

conflicting types error

I'm trying to make a smart irrigation using stm32f407 so, i used a Soil Moisture Sensors i write my code but when i trying to run the problem is :Description Resource Path Location Type conflicting types for 'Read_Soil_Moisture'; have 'uint16_t(void)...

Screenshot 2024-06-17 181149.png