User Activity

HelloI tried to implement I2S on the chip in question to send the data acquired by the on-board ADC (I tried both 8-bit and 12-bit) with DMA active on a curved buffer and half-word data size. The data should be read by an ESP32, connected to it on th...
Hello The STM32CubeIDE Version: 1.15.0 doesn't create the code for me because I can't login in the software persistently can't connect to the internet. I followed some advice found on this community thread https://community.st.com/t5/stm32cubeide-mcu...
Hello everyone.I have to create an arbitrary waveform generator via DAC starting from a lookup array of 32 elements at least with 10bit resolution. However, I must be able to reach frequencies of around 300Khz. I wonder, which evaluation board can I ...
Kudos from