STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Regarding USB Driver

Hello Everyone, I'm Bala! I'm New to the Embedded Field, In our Project I have to write one USB Driver code fully. This is where USB and Enum install, Endpoint Bulk transfer thing, Getting Device and Config Descriptor, and everything else comes in. S...

bsn_14 by Associate II
  • 2226 Views
  • 2 replies
  • 2 kudos

Resolved! Stop/Sleep mode for Low Layer lib

i am using STM32C011F6P6 and try to enter stop mode byLL_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);LL_LPM_EnableDeepSleep();__WFE();the current is little bit more than not entering the shutdown modeand the clock is not stoppingis there any thing I shoul...

STM32H5 FLASH_ECCDETR address decoding

In the FLASH_ECCDETR register, the ADDR_ECC field description contains:"The address in ADDR_ECC is relative to the flash memory area where the error occurred(user flash memory, system flash memory, data area, read-only/OTP area)."But I'm having troub...

PieterG by Associate III
  • 1882 Views
  • 1 replies
  • 0 kudos

STM32U585AII6 FMC cannot read and write PSRAM

Hello, I have a issue to control IS66WVE4M16EBLL-70BLI with STM32U585AII6. Although IS66WVE4M16EBLL-70BLI is 8MB, I can read and write only 8KB. IS66WVE4M16EBLL-70BLI has 22 address lines and 16 data lines.(4M * 2 = 8MB)     The problem is    if i ...

kongking_4-1718872404276.png kongking_6-1718872451878.png kongking_7-1718872567594.png kongking_8-1718872599895.png
kongking by Associate
  • 1131 Views
  • 0 replies
  • 0 kudos

Resolved! Reading I2c with sub-address

Hello All.Reading a register value from an I2C device assumes:  Writing the device address-> Writing the register address without STOP-> Reading the value . I am trying to figure out if I can do it using only available HAL functions but I don't see h...

baranovus by Associate III
  • 2532 Views
  • 2 replies
  • 2 kudos

Error in AN2834 rev 9

Hello ST people, I spotted an error in AN2834 rev 9, figure 8. Please refer to the image attached.A negative offset error should be depicted in figure 8, but it is a positive offset error, just like in figure 7. To be a negative offset error, the act...

ke1wa_1-1718781759126.png
ke1wa by Associate
  • 1871 Views
  • 2 replies
  • 0 kudos

Resolved! How to reset counter value ?

Hello everyone, i would like to know the HAL function that allows to reset the value of a simple counter. I don't find the HAL function to reset my counter to 0 before a next counting. So all i want to do is to count, read my counter value and reput ...

LHerm.1 by Associate III
  • 15548 Views
  • 6 replies
  • 2 kudos

Initialize the bootloader on STM32L432KC

I am a new embedded software engineer using STM32L432KC for my company's projects.I have been tasked to install a bootloader into this MCU. I am not sure how to proceed. I do understand that the BOOT0 pin which is grounded has to be set HIGH and BOOT...

Abijith by Associate II
  • 2493 Views
  • 5 replies
  • 0 kudos

Resolved! How to write multiple file in sd card sdio using fatfs

Hi, 1.I want to save multiple files but only 50 or 55 files savings.and how to save files next to next file.I want to fo fill data files up to to 32 GB.  2. how to reuse same memory for multi file creationint main(void){ /* USER CODE BEGIN 1 */  /* U...

pankaj4 by Associate II
  • 2498 Views
  • 3 replies
  • 3 kudos