Associate III
March 6, 2024
Question
Broken STM32
- March 6, 2024
- 1 reply
- 1274 views
Hi, I have a problem with a module based on STM32, more precisely it is a module that collects data from the ebike, i.e. temperature, speed, etc. This system is powered by an external 12 V converter, which reduces the voltage from approximately 80 V (20S battery). This converter is a ready-made module from Aliexpress. Coming back to my module, I don't know why, but after a few turn on/off cycles, the module stops working and burns out the STM. I have two linear stabilizers in the module, which respectively reduce the voltage to 5 V and 3.3 V. Is it possible that during startup (applying voltage to my module) voltage spikes appear somewhere, which burn the STM? I added the project schematics.