STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G030 debug in low power sleep mode

Hello,I've a project with the STM32G030F6 which the application use in 90% of time the low power sleep mode. In the reference manual page 95 is written that can debug:But in the register DBGMCU_CR dosn't exists a flag for the low power sleep mode. On...

bm2_0-1718957025921.png
bm2 by Associate III
  • 1505 Views
  • 0 replies
  • 0 kudos

Hard fault on Using FMC ram on stm32h753

I'm using a STM32H753 with external RAM. We were using it for LCD framebuffer. Now we are trying to migrate the stack and heap to the external RAM, when we run the code, getting hardfault on lines where std::array is declared. Any idea on how to debu...

sivaram by Associate III
  • 6445 Views
  • 11 replies
  • 2 kudos

STM32H7 CPU stall after RDP level change

I have an issue when changing the option bit of STM32H742 to change the RDP level to 1.I read out option bit from register FLASH->OPTSR_CUR, change the RDP bits to eg 0xBB, write the result to FLASH->OPTSR_PRG and then set bit FLASH_OPTCR_OPTSTART in...

Resolved! STM32Cube_FW_U0_V1.0.0 Version problem

I have recently upgraded CUBEIDE to v1.15.1I tried to add a example project to my workspace and it states Required Software PackageWhen I click next and finish, I get the errorI have checked for updates etc and tried to download manually using Embedd...

JK_lin_0-1718866570880.png JK_lin_1-1718866601530.png
JK_lin by Associate
  • 1565 Views
  • 2 replies
  • 0 kudos

Flash corruption and write protection mechanism

Posted on March 25, 2016 at 09:45We are using STM32F405 in our product which is a controller. We have met strange problems reported by our customer but can't reproduce the phenomenon in our lab when taking the controller back from customer. The cont...

BSMX falling edge data not always available

I am working on an application using an STM32U5A5 nucleo board with four MEMs PDM output format microphones. The microphones are configured such that data is valid for the left channel on a rising clock edge and valid for the right channel on a falli...

jcmoreau by Associate II
  • 1006 Views
  • 0 replies
  • 0 kudos

Resolved! Configuring STM32F439 timer to pulse at specific counts.

I wanted to use the STM32F439 timers, any of them but timer 8 seems to be the best one with my current peripherals, to act as a trigger source. Basically, the timer would drive a pin low, and at specific counts of the timer, drive the pin high for ~5...

EBDRS by Associate II
  • 7169 Views
  • 11 replies
  • 2 kudos

Resolved! LWIP Server FREERTOS

HI, my application is a tcp echoserver which works perfectly but, only for 10-20 minutes, after don't ping anymore. I'm using STM32H723 with LWIP and RTOS and I think it's a memory configuration issue. This is my setup: void MPU_Config(void) { MPU...

Stefano1 by Associate II
  • 1837 Views
  • 2 replies
  • 0 kudos