STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Communication between STM32C011 and EEPROM M24C0

Chào bạn,Tôi đã thiết lập kết nối theo sơ đồ và tôi đã tải mã trong tệp đính kèm nhưng tôi không thể đọc dữ liệu từ EEPROM. Địa chỉ M24C02 của tôi được đặt thành 0xA0.Ai đó có thể giúp tôi xác định vấn đề? Cảm ơn rất nhiều.  

HauDO_1-1718248224550.png
HauDO by Associate II
  • 6888 Views
  • 10 replies
  • 2 kudos

Resolved! VBus triggered by Data pins STM32H743?

I have a board that uses the H743 and have been having major problems with the USB side of things. I've only just realised that I left VBus floating all this time, so I'm assuming that's a major cause of my issues.. The board I have is designed as a ...

Resolved! External RAM for FrameBuffer on STM32H7S7L8

Good morning to all,I’d like to ask your advice.I have to insert an external RAM for the framebuffer because the internal one is not enough for LCD that I will drive (LCD-TFT LVDS 7 inch 1024x600).Which external RAM do you recommend? Could a QuadSPI ...

Leo99 by Associate III
  • 3612 Views
  • 6 replies
  • 1 kudos

Resolved! Error: No STM32 Target Found - But only in CubeProgrammer

Hello, I've been using the Nucleo-F446RE to program a stm32f4 series chip using the Nucleo's onboard ST-link capabiltiies. So far I have managed to get it to link and work in CubeIDE, but in CubeProgrammer it's giving me the following issue (attached...

raridi_0-1719501344798.png
raridi by Associate
  • 1447 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H723 / 733 / 735 analog temperature sensor vs. ADC Vref

Heyho,got my custom board running, only (minor) problem until now:internal analog temperature sensor (ADC3) value seems to be off, showing something like ~60°C,while an external sensor shows about 30°C."Finger test" confirms rather the 30°C.I have th...

LCE by Principal II
  • 4441 Views
  • 9 replies
  • 4 kudos

Resolved! Selecting Micro for touch display application

Hi,I have not developed graphic applications before and am trying to figure out how do I select an STM32 micro for a touch-display application using TouchGFX (if relevant to the question).The display I am looking at has an SDI interface and this is t...

Ricko by Senior III
  • 1430 Views
  • 2 replies
  • 1 kudos