STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UCPD and DBCC (dead battery) doubts

According to RM0456, p. 3459So in addition to CCx pins also PB5 and PB14 (DBCCx) cannot be used. The above does not make much sense to me. I imagine (only imagine) that internally DBCC support is implemented like shown below and for "dead battery" to...

TDJ_0-1719151138741.png TDJ_0-1719152739794.png
TDJ by Lead
  • 2677 Views
  • 5 replies
  • 0 kudos

Resolved! Long delay in setting TIM status register bits

Hi,I am trying to use CC1 and CC3 inputs on TIM2 of STM32H7A3 to do some time-critial tasks (very ns fast time-stamping). I need to identify which CCxIF tiggered. Using STMCUBEIDE the skeleton interupt code worked fine in debug mode without the lines...

HWhit.1 by Associate III
  • 1136 Views
  • 2 replies
  • 1 kudos

Resolved! ST Nucleo F767ZI USB not detected by PC

I've compiled my first program and I can't find a way to upload to the board.When I plug the USB, the onboard LED is lit, but my PC does not detect anything - I don't hear any "plug" sound, and I can't find any device in Device Manager (recognized no...

out_0-1719742246496.png
out by Associate
  • 2070 Views
  • 2 replies
  • 0 kudos

How to choose crystal speed?

I just was wondering how you guys proceed to choose an external crystal, specifically what speed it should have...The clock management with its tons of PLLs and dividers seems to be able to scale up almost any source to a desired frequency.for the L4...

b.a. by Associate III
  • 11288 Views
  • 16 replies
  • 2 kudos

Selecting GPIO in shared pins for STM32G030F6

In pins that share more than one GPIO, how do you set the GPIO to connect to the physical pin?For instance, for pins PA12/PA10 and PA11/PA9 one can remap them using SYSCFG_CFGR1 register. But is unclear for the rest of the pins. For example, TSSOP20 ...