STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Do I leak enough current?

Hello,I need to know what the minimum required current is to drive a pin as input for the STM32G0-series. I've gone through the datasheet but cannot find anything concluding for me. Could someone tell me?The reason is that I use a power switch to mak...

GOjayson_3-1714735297552.png
GOjayson by Associate
  • 1776 Views
  • 2 replies
  • 0 kudos

DMA Register Timer Input Capture STM32G431

Hi,I would like to measure the times and pulse lengths of an external signal from a GPIO. For this I wanted to use a DMA trigger (which writes the time points from the Tim to the memory).Here are 2 questions:1. where can I find a document that states...

pedahl by Associate II
  • 769 Views
  • 1 replies
  • 0 kudos

Resolved! How memory-mapped works on STM32L4?

Hello all,I am trying to implement an external loader for my board. Which uses a W25M02GV (QSPI NAND FLASH)I am following the https://github.com/STMicroelectronics/stm32-external-loaderI am trying to configure an STM32L4 to use this memory in mapped-...

djunho by Associate II
  • 4812 Views
  • 6 replies
  • 0 kudos

Resolved! HAL_Delay() stopped working

I have read most of the replies to posts that had the same problem that I am having with HAL_Delay() not working.  None of the solutions that I tried worked. It is apparent that the interrupt handler is never getting executed so any attempt to use HA...

Can DMA transfer directly to FMAC memory on STM32G4?

I want to use the FMAC to streamline weighted sum calculations using the FIR feature in non-circular mode. I have an array who's individual values are populated asynchronously via DMA and I use this array as the X1 buffer, but I missed that the buffe...

KHarb.1 by Senior II
  • 3427 Views
  • 7 replies
  • 0 kudos